Using the Mailbox Tab

Introduction

The Mailbox tab provides information about the currently selected units and the messages sent to and from those units. It is located immediately below the ViewPoint map, along with the following tabs:

The Mailbox tab shows position, tracking, status, configuration and text messages sent to and from the selected units.

Note: You can choose whether to display the tab, the columns to include and their order using the BASEBAR tab of the User Preferences page. You can choose the number of messages to display in the Mailbox tab using the Max Loaded Messages option in the DATA tab of the User Preferences page.

Most information in the tab is self-explanatory. See "Common Report Headings" for details of columns that may not be self-explanatory.

Note: ViewPoint stores messages for 90 days. You can view all of these messages by paging through while using History View. If you are using Live View, only the first page of messages is shown.

For messages sent from the unit, there is an icon in the column to the right of the OPTIONS button, which represents the status of the unit at the time of sending the message. For example:

normal_icon.bmp

There is a key explaining the meaning of the icon near the top-right corner of the Mailbox tab.

About message progress

Tab Options and Features

Message Types

CSV

LOCATE

Minimize and Restore

OPTIONS